I'm using an LM10CN as a simple voltage follower to buffer the input to a microprocessor ADC. I'm running the LM10 single ended from a 1.8 volt supply because this the the maximum ADC input voltage.
The load current should be tiny (a few microamps) but the LM10 output seems to saturate at about 1.13 volts, is this what I should expect when running from 1.8 volts or have I got something else wrong?
The circuit is trivial, a 10:1 resistor divider (18k/2k) on the input to pin 3, pin 2 connected direct to pin 6 for 100% feedback and supply connections and that's it.
Any suggestions or ideas would be very welcome.