Is there a plot of current noise density for the OPAX170? What is the input architecture (CMOS or Bipolar)?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a plot of current noise density for the OPAX170? What is the input architecture (CMOS or Bipolar)?
Thanks.
Phillip,
From the small magnitude of the input bias current (typical 8pA @25C), you may conclude that the OPAx170 is implemented on the high-voltage CMOS process. Since the input current noise spectral density is a square function of the IB, it is extremely small (few fA/rt-Hz) - see below. The increase in the current noise at f>10kHz is a direct result of the IB increase caused by input capacitance.