I have designed a low pass filter(of cut off frequency 20 Hz). I gave a sinusoidal signal of frequency 12.5 Hz as input to the filter. I connected the pin 6 of the filtering OPAMP to the CRO and I was satisfied with the output that I got on the CRO screen.
But when I connect the pin 6 of the OPAMP to the input of inbuilt ADC in MSP430G2553(to pin-P1.1), the output on the CRO gets disappeared.When I disconnect the pin 6 of the OPAMP from ADC input, the output waveform re-appears on the CRO screen. Any impedance mismatch problem?
From the datasheet of MSP430 ,the input capacitance is 27pF and a series resistance of 1000KOhm is present. I think I am correct about this information.
I have attached the TINA file of my filter along with the input impedance model of the ADC(using a 27pF capacitor and 1KOhm in series). I didn't find anything wrong with TINA simulation, but then Why am I not getting the output?
Thank you in advance.