Other Parts Discussed in Thread: TL331, LM7171
I am using TL331 comparator on my project5383.help for TI_TL33.docx. I am using it on simulation on pspice model that I obtain from TI website. I am using it to create pwm signal out put using TL331 components. I am trying to use TL331 components to create PWM. on the negative input side has pwm signal source and the positive side of the input 2.5 v dc. the goal is when negative input is smaller than the positive input then out put rises and stays at 15 v. until the negative input signal is smaller than the positive input signal. if the positive input is smaller than negative input, the output would be goes to zero. the problem I am having is when the negative input is smaller than the positive input, the output won't rise to 15 v right at the point. it takes about 2 micro second then it goes to 15V. I am trying to figure out why is doing that on TL331 pspice model. I used different model of comparator to see if the problem was the circuit. I used LM7171AIN and it works right. I was wondering if you would have any idea why is doing that. I would appreciate your help. thanks!]