Other Parts Discussed in Thread: INA219
Hi,
I am trying to use ina219 sensor (http://www.adafruit.com/products/904) with linux kernel driver on beaglebone black.
I want to use device tree overlay to use the sensor. I follow kernel indications (http://lxr.free-electrons.com/source/Documentation/devicetree/bindings/i2c/ina2xx.txt) and the sensor works as expected.
But adafruit board use 0.1ohms and default driver value for shunt-resistor is 10mOhms so return value are wrong.
I want to modify value in device tree as indicated
ina219@40 {
compatible = "ti,ina219";
reg = <0x40>;
shunt-resistor = <100000>;
};
but changing shunt-resistor value does nothing. The sensor is always create with 10mOhms value
ina2xx 1-0040: power monitor ina219 (Rshunt = 10000 uOhm)
How can i change the shunt-resistor value to get the proper return?
thanks,
Pierre