Hi.
I would like to know the difference between AMC1100 & AMC1200.
AMC1100 | AMC1200 | |
Isolation Mode Rejection 60Hz (Typ) (dB) | 108 | 108 |
Isolation Voltage Cont Peak (DC) (V) | 4250 | 4250 |
Isolation Voltage Pulse/Test Peak (V) | 5100 | 5100 |
Small Signal Bandwidth (Typ) (kHz) | 100 | 100 |
Gain Non-Linearity (+/-) (Max) (%) | 0.015 | 0.015 |
Operating Temperature Range (C) | -40 to 125 | -40 to 125 |
Best regards.