Hi, im trying to use the ina114 with a load cell
to use this I search in internet and I only find the same things, to make a wheatstone bridge with the load cells, put a 5v signal in to the bridge, when I do this i can read the output voltage with a volmeter (some few mV) it changes from 0.2mV to 0.8mV, but when i pass this signal througth the ina114, it gives me always the same voltge 4.33v.
this is the load cell that i use
http://proto-pic.co.uk/load-sensor-50kg/
this is the schematics
http://www.proto-pic.com/Resources/Application%20Example%20of%20using%20the%2050kg%20Load%20Sensor%20PPSEN-10245.pdf