Other Parts Discussed in Thread: INA122
I have two INA122 instrument amp circuits in series in a current loop with 4-20 mA. The first circuit in the loop has a 50 ohm resistor across pins 3 and 2 of the IA. The second circuit has a 40 ohm resistor across pins 3 and 2. Pin 5 Vref is tied to ground (pin 4). Vcc on the first IA is 24 VDC and 5 VDC on the second. No gain resistors are installed so the gain is 5. The second circuit in the loop works fine but the first circuit has a 0.1 volt offset on the output. What should be a 1-5 Volt output is 1.1 to 5.1. Any suggestions would be greatly appreciated.