Other Parts Discussed in Thread: TPS54062, ADS1120, TIPD125, DAC8750, XTR116
Hello All,
I intend to design a signal conditioning card for various field signals where I need to give standard 3 way isolation as shown in block dia. :
Input of the card will be 4-20mA signal from various transducers and output should be isolated 0-10V signal.
Here, my main concern is size and cost which I need to restrict to as low as possible.
One possibility can be using small DC-DC converters but it becomes a costly design.
I would appreciate your help if you have worked on something like this and share your ideas with me.
Thanks and Regards
shrikant.