This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

under the power supply of +5V, can PGA309 output absolute 0 v? or only output 60mV?

Other Parts Discussed in Thread: PGA309

on PGA309 zero offset:

under the power supply of +5V, can PGA309 output absolute 0 v? or only output 60mV?

  • Hello,

    The limiting factor of the PGA309 minimum output voltage is the output stage amplifier.

    With a +5V power supply, the output range is from 0.1V to 4.9V.

    The typical calibrated output voltage range of the PGA309 is from 0.5V to 4.5V to allow for overscale and underscale conditions.

    Best regards,

    Ian Williams
    Linear Applications Engineer
    Precision Analog - Op Amps