Other Parts Discussed in Thread: MPY634
Hi,
I want to use MPY634 for AM modulation. I used basic multiplier connection mentioned in MPY634 datasheet.
I have following issues:
1) When I connect carrier signal on X1 I become on X1 an input voltage offset of cca -0.2V. The input carrier signal measured behind C2 (see my connection) has no offset.
2) The AM output is very distorted and not behave like AM. When I change the input amplitude of carrier or MP3_in signal, there is only change in the amplitude of modulated signal. There is no change in modulation index. I need the standard AM like shown here:
http://en.wikipedia.org/wiki/File:Amplitude_Modulated_Wave-hm-64.svg
Please can you explain me what is wrong here?
Thank you.
Petr Duga
Here is my MPY634 connection:
Here are MPY634 signals:
where:
CH1: pin 1 (X1)- 900kHz, 1.04Vpp, -253mV DC, carrier
CH2: pin 6 (Y1)- 1kHz, 1.06Vpp, -16mV DC, MP3_IN
CH3: pin 12 (Out) - modulated signal