Other Parts Discussed in Thread: LM675, LM1875
Hello,
We have a few questions about the LM675. We are looking to convert 0~10V to 0~15V (gain=x1.5). We built a non-invert circuit on bread board and found if input voltage on non-invert pin was less than 0.75V, its output is saturated (at 13.77V). The OPAMP is operated at 15Vdc. This tells me I cannot convert 0~10Vdc to 0~15Vdc. I can only convert 0.78V~10Vdc to 0~13.77Vdc. Is there a way to resolve this issue?
Also, in the LM675 datasheet, it says, “The LM675 is designed to be stable when operated at a closed-loop gain of 10 or greater”. I am wondering if I pick the right part for my application?
In LM675 datasheet, there is a following example circuit. I build a simulation circuit with TI-TINA using OPA541E (because I cannot find LM675 simulation model in TINA). When I put 0.4V as input, the output current is not 2.5A. Why?
You can use voltage potential across output resistor R5, and divide it by the R5 resistance, which is 4 Ohm, to get the output current Io.
I attach my TINA simulation circuit for your reference.
Thank you!