Other Parts Discussed in Thread: AMC1100
Hello,
the output of the AMC1100 is Vdd/2 +-2V. So if there are +5V applied to the secondary side the output will be 2,5V+-2V. The problem is i need the signal as input for an ADC within a range of +-250mV.
Is it simply possible to apply +2,5V to Vdd and -2,5V to GND to get an output of 0V +- 2V ?
thank you