I am seeing what I would call a "permanent thermal shutdown" on several OPA549 op amps. That is, the OPA549 E/S pin is low (around 100 mV) when powered up and remains that way. The chip is always cool. I am using a single supply (+12V during testing) and have verified that everything is connected properly
I plan to ask for a failure analysis, but I am posting here to get a better technical understanding of how the thermal shutdown is implemented.
The schematics & layout of my board are available open source: https://github.com/jhu-cisst/mechatronics-boards/tree/master/QLA, in Altium Designer format and as a PDF; the motor driver circuit is on page 9 of the PDF.
A little more background: this is the 3rd low-volume production run of a quad linear amplifier (QLA) board that uses 8 OPA549 op amps. The first two production runs (qty 44 and qty 68) had no OPA549 issues. The third run (qty 72) had around 20 OPA549 failures (out of 72x8 = 576 op amps). I believe the soldering process was appropriate, with a temperature of 260 degC and lead contact time of 3-5 seconds.
I have found that if I measure the resistance between E/S and REF on a working OPA549, I measure 22-28 KOhms. The actual value depends on which multimeter lead (i.e., positive or negative) I connect to each pin, so I know it is not just a simple resistance, but anyway this seems to be an effective way to determine whether the op amp is good. For op amps in "permanent thermal shutdown" I measure many MOhms (essentially an open circuit). Conceptually, it is like there is a thermal fuse inside the OPA549. Can anyone enlighten me about the way this is actually implemented?
Although we have not identified any source of high (> 300 degC) temperature in the assembly process, I believe excessive temperature could damage the thermal shutdown feature. To test this, I took a working OPA549 and applied a soldering iron at 350 degC to pin 1, while monitoring the resistance between E/S and REF. Sure enough, after maybe 20 or 30 seconds, the resistance went from around 28 KOhms to many MOhms. And, it never went back down even after the chip cooled. So I think I successfully found one way to destroy an OPA549 and put it in permanent thermal shutdown, but perhaps there are others.
I am also concerned that some or all of the remaining (> 500) OPA549 op amps may have been damaged by whatever destroyed the 20 dead ones. Although they appear to work now, perhaps they will have a shorter life. Is there any way to test for this?
Any information is appreciated. Thank you.