Hi all,
My customer use OPA361Q1 and want it just as a buffer, 1:1. So I want to add a 2k resistor in serial with the inside input resistor 500ohm, and be a 1/5 attenuation. and then the total gain is 1:1
Another question is if we can just leave RSET disconnect? in older post, I see a same question post to ask RSET. I think it is OK, right? the output impendance of source is 75ohm.
Regards
Michael