Hi,
Does anyone have the data of LMV722 output voltage Swing for the condition below,
VCC+=5V, VCC-=GND, RL=1KΩ to VCC+/2, full temp range
We'd like to know the amximum voltage for VOL.
Thanks
Go
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Go,
The data sheet has 600 ohm and 2k data.
1k can be interpolated.
2kohm is [1.25mA,135mV], 600 ohm is [4.17mA,215mv], and 1k is [2.5mA,X].
x = 135mV + (215mV-135mV)*(2.5mA-1.25mA)/(4.17mA-1.25mA) = 169mV
169mV is maximum VOL because sinking current chart on page 6 looks linear between 1.2mA and 4.2mA
Hi, Ron
Thank you for your support.
Let me ask you one more thing.
If the load(RL) is placed between LMV722 output and GND,
I think that the minimun VOH value and maximum VOL value will become lower, is it right?
Thanks,
Go