This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

matching TI part for TSM109

Other Parts Discussed in Thread: TLV3011, TSM102

customer wants to replace ST micro's TSM109 to a compatible part.

What can we offer?

tsm109[1].pdf
  • Hello Stephen,

    TI does not have a direct drop-in for the TSM109. We do offer somewhat different comparators, but they would require circuit reconfiguration or other changes. The TLV3011/12 is a single comparator with a built-in 1.25V internal reference; it's not a dual device and not the 2.5V reference voltage of the TSM109. Also, it is intended for low supply voltages from 1.8 to 5.5V. We do offer some dual comparators with push-pull outputs that are usable with supplies up to 16V, but they don't  have an on-board reference.

    Regards, Thomas

    Thomas Kuehl

    Senior Applications Engineer

    HPA-Linear Products

    Texas Instruments - Tucson

     

  • Not drop in but look at TSM102.