Other Parts Discussed in Thread: MSP430F249, LMP91000EVM, LMP91000, LPV521, MSP430F2252, ADS1110, LMP91002
Hello,
I have an LMP91000EVM interfaced with a msp430f249 board.
I can fully control the LMP91000, read and write registers.
I can read the ADC conversion result, which fully matches VOUT voltage on the board.
External Vref 2.5V is OK and stable.
I have mounted a MICROceL HS sensor from CITY Technology. The sensor is in a dedicated connector, wires are as short as possible.
With the following configuration, Rload = 10Ohm, TIA Gain = 350K, Vref = 2.5V, Vref divider = 67%, I get VOUT = 1.697 V. Is this result realistic ???
Is this calculation correct: Iwe = (VOUT - 0.67 x 2.5) / 350K = 0.0628uA which is H2S = -1.6ppm
Do you have any experience with this MICROceL HS sensor ?
Is it possible to have a higher gain with TIA ???
Best Regards, Stéphane