Hi,
ABSOLUTE MAXIMUM RATINGS of 2nd page of Supply Voltage of the data sheet of OPA454 is 120V.
V+ of A1(and V+ of A4) of the 26th page of figure 76. of the data sheet is written as +100V.  
On the other hand, V+ of A1(and V+ of A4) of the 27th page of Figure 79. of the data sheet is written as +120V (ABSOLUTE MAXIMUM RATING). 
Is V+ of A1 of Figure 79. the answer that which of follows, (a) or (b) is correct?
(a) +100V
(b) +120V
I think that (a) is correct.
Regards,
Keishi Nishijima