Other Parts Discussed in Thread: OPA549, OPA548
Hello Everyone!
Our Application is to Control the speed of a DC Motor, without using PWM.
12V DC Motor that takes 2-3A current at full load.
The Input Volatge to the Amplifier will be in the range of 0-5V and it should probably be able to drive the said motor.
Can you suggest an Amplifier which will meet our specifications? I have checked out all the available OPAMPs in the High Current Amplifier Section! No, Amplifier gives an output voltage in the range of 9-15V!
Thanks!!