Other Parts Discussed in Thread: OPA690
Hoping you can confirm this application. Looking to power an OPA690 from +3.3V and -3.0V power supplies. The application is a low speed cable driver where the high output drive and disable features are important.
The amp is configured as a unity gain voltage follower with the + input DC coupled to the signal source. The input signal is a 5KHz digital signal swinging from 0v to +3.3v. TINA simulations all look fine. Do you see any issues that may not have been reflected in the TINA model?