This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2917

Datasheet for LM2917 did not have info on supply voltage.

Following are our design spec:

Frequency input is (0V-low, 24V-high), in range 4 Hz to 1600 Hz.

We can provide Supply voltage of value: 24V/12V/5V.

 Kindly suggest the suitable design parameters for LM2917 (R & C values).

Quick response will be appreciated.

Regards,

Sameera Simha.
GE HEALTHCARE

GA-SFW-280, 2nd Floor, Galileo, JFWTC, #122, EPIP,
Whitefield Road, Bangalore 560 066, INDIA
T: 91-8277336689.