Dear All,
I have a device which generate 0-75mV @ 0-10A, I mean when I have 0V it will have 0A and 75mV it will have 10A. I want to amplify voltage upto 5V but also decrease Ampere upto 250mA. Actully I want to measure ampere at periodically and keep watch on that it should not reach upto 0A. Is there any milivolt amplifier available? Please suggest.