Other Parts Discussed in Thread: LMH1981
Dear Sir / Madam,
We have few questions regarding to LMH1981
1 . In Datasheet, all timing Value(s) are Typical, no min. no Max.
We would like to get Min and Max, or at least Max timing parameters.
For example, we got series with TDhsout with delay in PAL 85ns instead 60ns (Room temperature, 24 Celsius)
2. No timing Parameter for OEOUT (Even Odd) , this signal is very important to us.
We measured OEOUT Delay:
Old board: 588 ns
New Board: 484 ns
In old board date code is VM23AB
In the new board date code is 41A57C
The parameter for CS out Typical is 525ns , I guess it’s same parameter for OEOUT, so once we got 588ns
Other date code 484ns.
Please be so kind and advise if you can provide those figures.
BR,
Nir