Hi I am pretty new at this kind of stuff but get the basics of it. I am working on a project that requires using an instrumentation amplifier but I cant seem to get a correct value for the gain I set. Currently I am inputting 100mv with a 5k resistor to set a gain of 45. I should be getting a value of 4.5 V but cant seem to get anything above 1V. I tried using a 500mv resistor as well and the same happens nothing above 1V. Im not getting something in my head that I should probably be considering but can you all help? I've used multiple breadboards, wires, and I have 10 INA122P's and its basically the same thing. Also with small inputs I get waves but all I get is square looking output waves if that helps any