Hi,
I am designing an ECG amplifier circuit using, for example, the INA122 (single supply).
Ive found a lot of information about amplifiers and filtering but finding info on a suitable power supply is a bit harder.
The device will be powered by a single cell Li-Ion battery.
My current line of thinking is using a something like the TPS61080DRC at 600kHz boosting the batt voltage to say 6V, then linear regs to take it down to +5V (TPS71701DCK) and +2.5V (TPS79901DDC).
Another alternative ive come up with is using a charge pump doubler and a charge inverter with a couple of lin regs to get +5V and -5V but the output impedance of these devices coupled with having decent headroom for the lin regs meant that this method was a headache...
Can anyone give me any advice on this? Im sure it's a very common problem.
Thanks,
Tim