Other Parts Discussed in Thread: OPA336, LM358
Bill,
This reason that you have not found any literature on driving the output of single supply amplifiers to ground is that it is not recommended. I know that you have placed a diode at the output and you are trying tricks to pull the output down to ground however you may see significant linearity problems near ground.
There are some single supply amplifiers that will get you close. The OPA336 comes with in 3 mV from the rail ( http://focus.ti.com/docs/prod/folders/print/opa336.html ). With this device you will get close to ground but you may still have linearity problems lower that 200 mV.
Typically, designers boost the signal going through the amplifier with a level shift of some sort. You can use the reference of the ADC to accomplish this. I do have some circuits that will help you accomplish this if you are interested. Please let me know.
Bonnie Baker
Sr. Applications Engineer
Data Acquisition Products
Texas Instruments, Tucson
From: William Twomey [mailto:w.twomey@gmail.com]
Sent: Friday, October 23, 2009 5:32 PM
Hello Bonnie,
I'm a fan of your EDN articles and am currently reading your book - A Baker's Dozen - which I have enjoyed so far. I appreciate that your EDN articles dive into real world and issues and have some real substance to them.
I have a general question about using single sided op-amps as ADC buffers I was hoping you could shed some insight on. I like using single sided rail to rail amps in front of ADCs to protect them from over/under voltage without the use of extra protection circuitry. The signals I commonly deal with, however, need to be read accurately down to ground. Since the output of single sided amps have trouble reaching ground, I'm thinking that I can use a diode on the output of the amp with the feedback connected after the diode to force the output of the amp up ~0.6V, well into its linear region (I'm not concerned up the drop in the upper output limit). I was also planning on using a weak pull down resistor after the diode to help the output touch ground.
I figured this would be a common practice and have looked around for AP-Notes or articles discussing such a method but haven't really found anything. This makes me a little nervous and so I'm wondering if I'm missing a big negative or drawback to this approach. I ran a PSPICE simulation and the concept seems to work but I know real world results can be different. Is there anything I'm missing? Any insight would be greatly appreciated,
Thanks and Best,
Bill Twomey