This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3501 & OPA357 schematic review

Other Parts Discussed in Thread: TLV3501, OPA357

5657.AC Voltage Detect_OPA357_29002504.pdf2376.TLV3501&OPA357_29002511.pdf

Hi all,

These are the oscillation circuit(TLV3501 & OPA357) and the circuit for voltage detect.

 The oscillation circuit: 6.78MHz, 0.3V~3V Swing, Ref=1.65V

Comparator: AC voltage detect, using the function of 6mV hysteresis of comparator

I would like to know that the value of resistors is proper as well.

Could you review these schematic circuit?

Thank you.

 

Best regards,

Sammy Jeon.