Other Parts Discussed in Thread: TLC251, TLV2370, TLV2460
In Single-supply mode with VDD=12V, Vdd- at GND, and set for "High-bias mode", What output current can this opAmp drive a 10K load to ? Can it drive a 10K load to 10v at 1mA ? Doesn't look like it can do it, since typ Idd is 1mA in high-bias-mode. The 18-page datasheet does not seem to cover its output drive ability in a direct fashion.