Other Parts Discussed in Thread: OPA1632
Hi!
OPA1632, pin 2, what is the input characteristics of this input? Can't find anything in the datasheet.
Have I understood it right: This input makes the outputs be centered around the voltage at this pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA1632
Hi!
OPA1632, pin 2, what is the input characteristics of this input? Can't find anything in the datasheet.
Have I understood it right: This input makes the outputs be centered around the voltage at this pin?
Hi Peranders,
You are right. But there is a little bit more to it.
Vocm sets the output common mode voltage, the voltage level around which the output voltage is centred.
By default it is set to Vcc/2 where Vcc is the supply voltage, if it is required to be at the same level, then Vocm should be left unconnected.
If you require a dc shift in the output voltage ,then you need to apply the required voltage level from an external voltage source to the Vocm pin. It also requires a 0.1uF decoupling capacitor to filter out any high-frequency noise.
Regards,
Sid
Hi peranders,
Actually Vocm just sets the DC voltage level around which the OUTPUT voltage is centred.
The peak to peak level of output voltage is the same. Its just that this output voltage is offset by the voltage given to Vocm. This offset voltage should not need any specifications because it mainly depends on what device you are using at the output of OPA1632. You can have the dc offset as 0V, 1V, 5V, 10V ,etc.. as long as it is sustainable by the device to which this output voltage is fed. The peak to peak output voltage is still the same.
So, I think the specifications are not mentioned because they can be variable depending on the output device.
Hope this helps.
Regards,
Sid