Other Parts Discussed in Thread: TL431, LM324
We are designing constant current source , circuit as shown in TI application note AN-1559 Practical RTD interface solution. (Refer Figure 2 page 4) . link : http://www.ti.com/lit/an/snoa481b/snoa481b.pdf
We are designing circuit using TL431 as reference ( 2.5V refernce ) , LM324 OPAMP , R8: 2.49K .
R6 = R10 = R9 = R7 = 22K . Single supply for OPAMP 5V , 100 ohm resistor is connected as Load .
Expected : Current through R8 is 1ma ,
Observation : Refernce Voltage generated : 2.496 V , Voltage Across R8 : 2.86V : Current through R8 1.15 ma ,
Question :
1 ) Why Voltage across R8 is not 2.5V ? Is any changes required in value of R6,R10,R9,R7 ?
2) On what basis the value of R6,R10,R9,R7 are desided ?
3) By only changing R8 what will be range of Constant current that we can design ?