Can anyone confirm the drop in replacement for the 4136 as being the TL075 or the TL075CN? Also, what does "CN" mean?
Thanks,
Tony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Tony,
I've moved your post to the Precision Amplifier forum where these parts are supported.
-d2
Hi Tony,
C: Comercial Temperature Range (0 to 70oC)
N is the package naming. It shows the package in the dataseet.
The TL075 is actually the same device as the TL074, but with different pinouts.
If you are looking for drop-in device, then the RC4136 (I assume you meant RC4136) will be your choice.
Thanks,
Ying