This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Driving stepper motor using uln2803

Hello! I have been trying to drive a stepper motor with the following specifications: 4V and 1.2A and 1.8 degrees per step with uln2803 but I am unable to actually rotate..that is turn it CW or CCW.. the motor just vibrated but the shaft does not rotate.

But on the table it vibrates with which the motor turns CW .

I would be very glad if my problem is solved.