Other Parts Discussed in Thread: LMP2022
For any linear amplifier with 2 inputs V1 and V2 : output V0=A1V1-A2V2+Constant.
For an opamp A1 >0 A2 >0 A1approximately = A2 but A1can be < A2 or A1 >A2
If we define : Vcm=(V1+V2)/2 and Vd = V1-V2 then V0= A1.(Vcm+Vd/2) - A2.(Vcm-Vd/2) +Constant or
V0=(A1-A2).Vcm + Vd/2.(A1+A2)+Constant = Acm.Vcm+Ad.Vd+Constant
So, the common mode gain Acm = A1-A2 can be >0 or <0 and CMRR = Adm/Acm can be >0 or <0.
Do you agree with this conclusion?
Of course CMRR in db = 20.log( absolute value CMRR) always >0
For a dual output LMP2022, I suppose that the polarity of the CMRR of each half LMP2022 is independant of the polarity of the other half LMp2022?
Do you agree with this conclusion.
I need to know because in my circuit an output is dependant on the difference of both CMMR.
An other output is dependant on the sum of both CMRR.
Thank you for your effort.
Marc Windels