This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Instrumentation Amplifier Output Offset



Greetings,

I am building a very simple circuit.  I need to take a 0V to 1V signal and produce a -5V to 5V signal.  I would like to do this with one of the INA series instrumentation amplifiers.  I feel it would be easiest to have one of these units produce a gain of 10 and then offset the signal by 5V.  Can this be accomplished by connecting a -5V reference sourse, i.e. a negative linear regulator, to the reference pin of the amplifier in order to bring the signal down or should I simply ground the reference pin and connect the output to a difference amplifier with unity gain?  Thanks in advance for the help!

-jim