Other Parts Discussed in Thread: INA129
I am using an INA129 (http://focus.ti.com/lit/ds/symlink/ina129.pdf) in the ECG set up shown on the bottom of page 11, with a 47 pF capacitor added in parrell to the 390k Resistor in feedback on the last stage of the right leg drive. I have also added an additonal gain stage with around 50 v/v as well as a DC restorator. However, at the output of the IA I am seeing a DC offsetof -1.07V (consistantly). This persists regardless of the gain, and regardless of the input signals. This is resulting in heavy saturation of the rest of the circuit. Can anyone help?