Other Parts Discussed in Thread: PGA309
Hello,
We are having a little trouble with the Multi-Cal System for the PGA309 I have been looking for the source code and have not been successful. The software I am using is sboc401a is this the newest version? What would the D-Sub pin out be to hook up the sensor to the D-Sub 9 connector? When using the program if I set the first temperature to 37.7°C it asks to set the temperature to 0°C am I not setting it up right, also is there a way to set it to °F?
Thanks,
Jim