Hi,
I'm developing a transimpedance amplifier with very high bandwidth (about 100MHz) for very low capacitance photodiodes. I've previuously used the LMH6624 with good results, but want to try the OPA847. To get an idea of the noise performance, I'm testing a stripped-down configuration, i.e. just the op-amp with a 5k feedback resistor in paralell with a 0.1pF capacitor (plus parasitics). With LMH6624 this gives results close to what I expect. However with an OPA847 I get much higher noise than expected, even at only 10MHz, and going up to peak around 95MHz.
This looks as if there was a massive input capacitance at the inverting input pin - around 25pF would explain the noise I observe. However I can't image where this should come from. The board works as expected with LMH6624, and the specified OPA847 input capacitance is only a few pF larger than LMH6624. I'm really at a loss what's going on here.
Any thoughts appreciated!