This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4508 output swing

Other Parts Discussed in Thread: THS4511, THS4513, THS4508, THS4509

In the THS4508 datasheet SLAS459E - rev Sept 2008 - Fig 30 shows VOD swing vs Load Resistance.  The x-axis is labeled "RL - Load Resistance - k-ohms".  Is this a typo?  The THS4511 in the same family has the same label, but the THS4509 and THS4513 are labeled ohms.  Everything in the datasheet, including the Test Circuits and Applications circuits discuss 10s - 100s of ohms for load, but not 10k - 1M.  These values don't seem reasonable.

  • Hi Robert,

    I think you are right. The x-axis in THS4508 and THS4511 should have the axis in ohms, instead of kohms by mistake. Thanks for catching this error. We will plan on correcting this mistake on the next revision.

    Best Regards,

    Rohit