Hello,
i need help with design of the transimpedance amplifier for photodiode and ADC for the purpose: we have a TOF camera which works with IR light, the problem is that the IR source of light placed around the sensor and when you put the camera behind the double glassing, the camera sees nothing due to rereflection of the IR light directly to camera. After taking aut the IR source of light and putting it on 20cm far away from camera, the system starts to work. The goal is to create external source of light in order to solve the problem.
The laser frequency should be synchronized with original source of light as much as possible, and there only one way how to trigger the frequency, it is photodiode. For this purpose I took Osram FH 2400 with capacitance 11pf and switching time 5ns which should be sufficient for this task. Then I checked possible operational amplifiers and have chosen the OPA656. For Laser Driver I took iC-HG laser driver(same as used inside of the ToF camera). Now I'm a bit stuck due to lack of knowlage with the question of the whether I'm right with OPA, if right what transimpedance gain and feedback capacitance should I use for it. I also need to find proper ADC with MCU, and can it be combined in one package?
Thank you very much in advance!