This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2365 - Sallen-Key HP continous saturation

Other Parts Discussed in Thread: OPA2365

Hi,

I would like to implement a 4th order sallen-key hp filter with two gain stages to filter/amplify an ultrasonic signal at 200kHz. The filter-incoming signal level rises continously and I need high gain particulary on the first few incoming periods which means that at a high gain later (in time) incoming signal-periods, at a high signal level, will force the op amp to go into saturation. This from the signal processing point of view is not a problem but I wonder if it would harm the op amps (OP2365) if they are forced to saturation in continous operation over years?

Thanks.

Best,

Rob.