Dear all,
I'm using an LMH6624 for a high speed transimpedance amplifier. The topology is pretty simple:
- input photodiode
- feedback resistor (which sets the gain) capacitor (to increase the phase margin)
- the positive input of the OpAmp is connected to ground
With a 1Kohm resistor and a ~10 pF capacitor to compensate I get a flat frequency response up to 60/70 MHz. (see attached picture)
That is basically ok but all of a sudden there is a peak at 250 MHz that can't be explained from the information in the datasheet.
Does anyone have any idea about what could cause this?
Thanks a lot in advance.
Best regards