Hello,
I need to interface an analog hall effect sensor to ADC ( F28M35H52C controller) which is 10 meter away. Design Specs are given below.
Sensor: SS39ET/SS49E/SS59ET Series Hall effect sensor.
Output: Sine wave whose magnitude varies from 1V to 4V (1V DC offset), 300Hz Maximum frequency. Supply Voltage: 5V
Controller: F28M35H52C, ADC reference supply: 0 to 3.3V
As per my understanding, one options is to use Op Amp buffers which can drive high capacitance cables ( Consider 1uF ).
Kindly suggest the OP-Amps / Designs for my application. Also suggest better alternative if required.
Thanks in advance,
Regards,
Govind.