My problem is to analyse the 3rd order harmonics which present in the HVAC line.
after that HVAC line(60Hz) ,MOV(Metal Oxide Varistor) will present to avoid the flow of high current to the components which is connected in the AC line.(eg.Surge Counter).MOV life span will be degraded day by day.Thus leakage current flows through the component. To analyse this we added voltage divider next to that and after reducing the voltage, we need to add filter circuit to pass 180HZ alone with minimum BandWidth. For that I followed Band Pass Filter with Sallen Key Topology.
I have attached the filter circuit with output using TINA software.