please tell us how to treat the unused part/pin of ths6226 ?
for example, I can leave the part AB without power or better off via serial interface and leave pin floating? if I can leave it without power, as is powered serial interface?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
please tell us how to treat the unused part/pin of ths6226 ?
for example, I can leave the part AB without power or better off via serial interface and leave pin floating? if I can leave it without power, as is powered serial interface?
Hi Marco,
I would better apply the supplies for ports AB and power down the port AB via the serial interface and leave the pin floating. The serial interface is powered ON via the port AB supplies.
Also, I would keep the supplies and connections for the unused port as it is mentioned in the application section of the datasheet as you might need it for future purposes.
Best Regards,
Rohit