Hi Team,
Our customer is considering to use THS7303 or THS7353 as a replace of a video filter device. There are many typical application example in the datasheet which have several value for input and output AC coupling capacitor. How do you choose these input/output AC coupling capacitor value ? Customer is willing to use smaller value than the example(470uF, 47uF) in the datasheet. If there is an equation, could you please share us the information ?
They would not use sync tip clamp or sag correction function, only as an filter. If the device is used just as a filter, I believe there would not be a big difference between the two devices.
Best Regards,
Kawai