Hello. My circuit uses a XTR110 to translate a voltage signal from 0-10V to 4-20mA, using the basic circuits from its datasheets, with a P-MOS at the output to drive the load.
I need that the output current be 0mA when a fail is detected in other sections of the system. The fail signal is CMOS/TTL.
In the image below I propose an implementation based on the Ouput Enable circuit from the XTR111 datasheet. The switch would be implemented with a small signal MOS transistor, with its gate controlled by the fail signal previuosly mentioned. My concern is about the 3k resistor in the gate of the Qext transistor, how it will affect the control loop from the XTR110.
Reeplacing the XTR110 for a XTR111 is not an option (for now). The input signal range can be modified if needed.
Is there another more elegant solution to implement a ouput enable/disable for the XTR110 to indicate a fail in the system?
Best regards,
Mr. Electron.