Other Parts Discussed in Thread: XTR115, XTR111, XTR110, XTR117
I am thinking to use XTR115 for a 3-wire 4-20mA system as follow, will it be all right?
I prefer XTR115 over XTR111 since it requires much less external components.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joshua,
You can't use the XTR115 as a three wire transmitter, it simply will not work. Consider the XTR110 or XTR111 when designing three-wire 4-20mA transmitters.
I wrote a blog about the issue this will cause which you can read here:
Here's parts 1 and 3 if you're interested in further reading:
Here is a TI reference design using XTR117 in a 3-wire current loop. Wondering if XTR115 can do the same?
www.ti.com/.../tidr225.pdf
Hello Joshua,
The schematic you've attached clearly shows that the XTR117 is used as a two-wire transmitter. The two connections to the transmitter are Loop+ and Loop-. The XTR115 would work in place of the XTR117 is the schematic you've attached.