Other Parts Discussed in Thread: LM675, LM1875
Hi -
I'm running a pair of LM675's as a differential output driver at 70 khz at up to +/- 20V peak sinewave output from +/- 24V supplies. Each is running at about 23db gain closed loop so there wouldn't seem to be a stability issue although my circuit is somewhat different than the simple example circuits in the spec sheet for the part.
The problem is that each of them are dissipating about an amp internally under these conditions and the customer is rejecting this lack of efficiency.
This extremely high current remains constant even with no load which appears extremely strange and wasteful for an amplifier claimed to have a 70 Khz power bandwidth, which is how I am operating it.
The heat problem appears to get linearly worse as frequency increases above 10 khz, and the amplitude exceeds about 20%. When with no output level or at much lower frequencies, the LM675 appears to be in spec current wise.
I can supply a schematic to show exactly how I'm operating them.
Is the LM675 actually this inefficient? It appears to be hugely wasteful to waste 24 watts as heat @ 70 khz below clipping. with no load at the output.
Btw, it appears likely that the 1 ohm, 0.22 uf stabilization network is the major culprit here. In the lack of margin of stability characteristics in the product spec, what might TI suggest as an alternative stabilization approach to allow the LM675 to meet its claimed performance as a ''70 khz full power bandwidth amplifier' while maintaining a reasonable level of efficiency up to 3A?
You can reach me at tom.dawson@siliconengines.net or by phone at 224-795-5372.
Thanks Tom Dawson