The datasheet doesn't show LONG-TERM STABILITY for REF3325. Do we have such data?
Regards, Bernd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bernd,
We do not have the Long Term Stability data for REF33xx to share with you BUT as part of the initial qualification all new products must pass a lifetest (an accelerated aging process in high temperature ovens) that requires maximum shift of the parameters like the initial accuracy to be no greater than the max/min spec shown in the PDS. Therefore, in case of REF33xx with the initial max spec of 0.15%, the maximum shift after 10 years is no greater than 0.15% or 1500ppm.
For more details on the topic of long-term stability, please read my blog below: